SDK Operation
ROS Simulation
① Set ros workspace
If the user is not familiar with the path setting, please create the folder named unitree_ws/src and move folder unitree_ros folder in it, which shoud be ~/unitree_ws/src/unitree_ros. Then download the folder unitree_legged_msgs, move it to ~/unitree_ws/src/.
cd ~/unitree_ws #Open the folder
catkin_make #Initialize ROS workspace
echo "source ~/unitree_ros/devel/setup.bash">>~/.bashrc #Add the ros path to the environment variables
source ~/.bashrc #Update environment variables
Run roslaunch unitree_gazebo z1.launch, If successfully configured, the simulation interface of Gazebo will be displayed.
Tips:After entering `RosLaunch Z`, press tap to check whether the terminal will automatically complete. If rosLaunch Z1_ is successfully programmed, that means the path setting is successful.
② Open the CMakeLists in the z1_controller folder and change the compilation conditions as follows.
# set(COMMUNICATION UDP) #UDP
set(COMMUNICATION ROS) #ROS
③ Compile z1_controller, create a folder named build in this file (open the second terminal).
mkdir build
cd build
cmake ..
make
Execute the executable file ./z1_ctrl in folder build. The default control mode is SDK, if you need to use keyboard control, use ./z1_ctrl k
When executing this command, the terminal will continuously print statements, such as[WARNING] UDPPort::recv, unblock version, wait time out, this is normal because we have not started the robotic arm SDK to communicate with the robotic arm controller.
Various information will be printed in this window, please observe the content of this window.
④ Open folder z1_SDK and create folder build in it (open the third terminal).
mkdir build
cd build
cmake ..
make
Execute the executable file in folder build.
There are two executable files generated, example_lowcmd_send and bigdemo.
This time we run bigdemo.
./highcmd_basic
- Keyboard Operation:The specific keys will be introduced in state machine section.
First press 2 on the keyboard and then press key 0, the robotic arm will enter the label operation state machine. Input forward at the prompt, then click enter, the robotic arm will run forward. Press ~ again, return to the origin. After returning to the origin, it will automatically enter the joint control mode. At this time, the rotation of the robotic arm can be controlled by long press according to the following keys.
| Joint ID | 0 | 1 | 2 | 3 | 4 | 5 | Gripper |
| Keyboard | Q/A | W/S | D/E | R/F | T/G | Y/H | up/down |
Joint Action (right hand) | positive/ negative | positive/ negative | positive/ negative | positive/ negative | positive/ negative | positive/ negative | positive/ negative |
Now, we have completed the simulation operation. The whole process is: Run ROS–>Run z1_ctrl–>Run SDK instance.
Real Machine Control
① First power on the robotic arm, and check whether the communication is normal by ping 192.168.123.110 command.
② Open file CMakeLists in folder z1_controller and change the compilation conditions as follows.
set(COMMUNICATION UDP) #UDP
# set(COMMUNICATION ROS) #ROS
③ Run ./z1_ctrl ④ Run ./highcmd_basic
The operation here is consistent with the simulation. Now, we have learned how to control the robotic arm. More operation methods will be introduced in the basic concept section.
Multiple robots control
<1> open the directory z1_controller, set Communication in CMakeLists.txt to UDP,
copy the directory z1_controller, named as z1_controller_111
<2> open the directory z1_controller_111
① main.cpp
set UDP port (Line51) as shown in the following example:
ctrlComp->cmdPanel = new ARMSDK(events, emptyAction, "127.0.0.1", 8074, 8073, 0.002);
② config.xml
set IP to "192.168.123.111", set Port to 8882
③ unitreeArmTools.py
set the second robotic arm IP to 192.168.123.111.
<3> As described previously, proceed as follows:
- execute z1_ctrl in z1_controller at the first terminal, which communicates with the robotic arm 110.
- execute z1_ctrl in z1_contrller_111 at the second terminal, which communicates with the robotic arm 111.
- execute lowcmd_multirobots in z1_sdk at the third terminal.
And then we can see that the Joint1 of both robotic arm has turned at an angle.