Introduction to SDK
Three files are provided for users to use z1 robot, which are z1_controller, z1_sdk and unitree_ros.
- z1_controller: which stroes the code to control the z1 robot directly.
- z1_sdk: which contains the interfaces used for z1 robot control.
- unitree_ros: which contains the unitree products, includes Go1, A1, Aliengo , Laikago and z1 simulation files.
1. z1_controller
Apart form the files mentioned below, users do not need to view other files under this folder.
1.1 build/z1_ctrl
For the first time, users need to create "build" file and compile the program, and the resulting executable program is named z1_ctrl.
- execute
./z1_ctrl -vto check the version information - execute
./z1_ctrl kto control the robot by keyboard - execute
./z1_ctrlto control the robot by SDK
1.2 build/sim_ctrl
If gazebo has been installed then there will be a executable program named sim_ctlr, which is used to communicate with unitree_ros. Other than that, it has no different than z1_ctrl.
1.3 unitreeArmTools.py
This file is used to change the lower machine IP address (default: 192.168.123.110)
Use a cabek to connect the robot (which needs to connect to the right backup network port) and PC, then execute python3 unitreeArmTools.py and enter command as prompted.
1.4 config/config.xml
This file is read only once when z1_ctrl starts.
-
IP & Port
IP:This refers to the robot lower machine IP address changed by
unitreeArmTools, and when it has been changed, this parameter should be changed at the same time so that thez1_ctrland the robot can communicate normally.Port:The port of the robot is 8880, and this parameter is to change the native port bound when the PC performs the
z1_Ctrl, the defalult is 8881, which is used to control multiple robots on the same PC. -
collision
settings for collision check
open: Whether open collision check by selecting Y or N
limitT: The difference between torque and feedback torque , which calculates for collision check
load: The end load is attached to the end joint, which affects the calculation of the feedforward torque, and it is always in effect.
1.5 config/saveArmStates.csv
This file is to save label for labelRun() and labelSave(), which represents the joint angles at that position.
2. z1_sdk
2.1 include
The forlder holds the header files of unitree_arm_sdk, and users can view the comments in it to understand what function does.
2.1.1 unitree_arm_sdk/control
There are two files in it: ctrlComponents.h and unitreeArm.h.
ctrlComponents.h mainly puts all the control parameters in a class for easy calling.
unitreeArm.h encapsulates all interfaces for controlling the robot.
2.1.2 unitree_arm_sdk/model
This folder contains the armModel class, which contais functions suchas forward and inverse kinematics, inverse dynamics, and spatial Jacobial calculations of the robot.
The user can use these functions by calling _ctrlComp->armModel in the class unitreeArm.
2.2 examples
This folder contains three examples for the use of the unitree_arm_sdk.
2.2.1 highcmd_basic
If the user just wants to a simple understanding of how to control the robot, they can check out highcmd_basic file.
The example contains three methods for controling the robot.
① armCtrlByFSM()
The function controls the robot by calling the methods in the class unitreeArm directly, such as MoveJ(), MoveL(), MoveC(), backToStart().
The function work as if the user use keyboard to control the robot with the ‘./z1_ctrl k' command.
② armCtrlInJointCtrl()
The function is equivalen to further encapsulation on the basis of highcmd_decelopment. The user is only to control the direction of joint rotation instead of entering joint command \(q \And \dot{q}\).
The following command calculation will be performed directlu in the function:
\(\dot{q} = directions*\omega\)
\(q_{k} = q_{k-1} + \dot{q}*\delta t\)
And the function is equivalent to pressing 2 key when control by keyboard.
③ armCtrlInCartesian()
In cartesian space, the user was originally required to control the sptial velocity \(V = [\omega \quad v]'\), that is, unitreeArm.twist to control the robot, and the function was encapsulated on this basis. Then the user can directly control the direction in which the end of the robot was desired.
The following command calculation will be performed directly in the function:
where T is a homogeneous transformation matrix composed of R and p, and [ω] is the antisymmetric matrix of ω.
\(posture_k = posture_{k-1}+posture_{\Delta}\)
\(T_k = T_{\Delta} + T_{k-1}\)
\([\omega] = \log{(R_{k-1}^T R_k)}\)
\(v=p_\Delta\)
And the function is equivalent to pressing 3 key when control by keyboard.
2.2.2 highcmd_development
If user wants to control the robot through the planning trajectory, they can view this example.
When sendRecvThread->start() executes, the thread executes arm.sendRecv() at a frequency of 500HZ.
When controlling under the joint space, this function will send q, qd, gripperQ, gripperW in unitreeArm to the z1_controller, When controlling under the cartesian space, the function will send twist in unitreeArm to the z1_controller, and the user only needs to keep changing these parameters to control the robotic arm. You can also write your own thread to call unitreeArm.sendRecv().
2.2.3 lowcmd_development
If the user wants to control the \(q, \dot{q}, \tau_f, k_p, k_d\) parameters of the motor directly, they can view this example.
This file shows how to send PD parameters directly to the motor. Users can control the motor by writing their own program to achieve independment development. The final output torque of the motor is as follows:
\[\tau = k_p * 25.6 * (q_d - q) + k_d * 0.0128 * (\dot{q_d} - \dot{q}) + \tau_f\]25.6 and 0.0128 are the scaling multiples in the communication protocol with the motor.
The sendRecvThread under CtrlComponents is a function that calls unitreeArm for instruction operations, such as running to forward as an instruction
And when running lowcmd, it is recommended to use its own defined thread, execute the run function, the run function starts to determine the command that needs to be sent to the motor through calculation, and finally calls sendRecv to send UDP packets.
2.2.4 lowcmd_multirobots
This program provides example of controlling munltiple robotic arms.
For more information, see SDK run
2.3 examples_py
This contains the Python version interface of the z1 SDK.
The interface is designed in the arm_python_interface.cpp file, and the functions and variables already included in it can be used directly in Python, and users can also change them by themselves, see for details pybind11 documentation
invoke method:
There will be a library named unitree_arm_interface in z1_sdk/lib after compilation is complete.
Execute ./z1_ctrl in the first terminal.
Open a second terminal in the z1_sdk/examples_py directory to execute python3 example_highcmd.py